You’re Paying Too Much for Energy… No, Really
The low cost of crude oil has suppressed natural gas and electricity prices. Energy is unusually cheap — right now. So, from a purchasing perspective, nothing to see or do here, right?
Not true. The actual energy used to power a facility or any type of operation accounts for less than 50 percent of a utility bill. The other half of the pie, known as non-commodity charges, continues to increase. Check out this breakdown of an average invoice showing the real cost of energy and where potential savings exist.
Download the infographic.
And click here for more information on building a strategic sourcing program.
The post You’re Paying Too Much for Energy… No, Really appeared first on Schneider Electric.