ESPC Enables Energy Resilience at Moody Air Force Base
Learn more about Schneider Electric's $22.6 million grid stability and energy efficiency project with Moody Air Force Base (Moody AFB) in this video interview with Air & Space Forces Magazine.
Leveraging its federal ESPC experience working with military bases including Fort Huachuca, Naval Base Coronado, and Yokota Air Base, Schneider Electric worked with Moody AFB to install a comprehensive energy project. Schneider Electric installed a new 2.5-megawatt solar array, which is now providing the base with clean, renewable electrical power while offsetting the utility bill. Moody also received an expanded, cyber-secure energy management control system, which makes energy usage levels more visible while improving indoor air quality and occupant comfort.
For more information about Schneider Electric’s work with federal agencies, visit perspectives.se.com/federal