What Is the Difference Between Direct and Financial (Virtual) Power Purchase Agreements (PPAs)?

December 24, 2020 Jenna Bieller

As the market for voluntary renewable energy buyers matures, commercial, industrial and institutional (C&I) buyers need a deeper understanding of how corporate renewable energy procurement differs from traditional energy sourcing strategies. Power purchase agreements (PPAs) are the most impactful route large corporations with clean energy goals use to reduce operational emissions. However, navigating PPA contracting and negotiations comes with a steep learning curve for corporates first entering the field.

The main component of this learning curve is to understand PPA deal structures. There are two main ways that a PPA can be structured: direct (also known as retail-sleeved or physical) or financial (also known as virtual or synthetic). The degree of climate impact and economic favorability of the deal depends on the type of PPA structure an organization chooses.

While these deal structures produce a similar result — a long-term contract between a renewable electricity supplier and a creditworthy offtaker — there are several important differences that corporate buyers should be aware of.

Direct vs. Financial PPAs

A direct PPA is an agreement made between a renewable energy generator and an end user in which electricity produced by a wind or solar facility is physically delivered to power the corporate buyer’s operations. Because the corporate offtaker actually takes title to the energy produced in this type of deal, the final price for delivered power is a function of the contracted PPA price plus transmission-related expenses.

In exchange for agreeing to offtake power for a fixed amount of time, corporate buyers of direct PPAs lock in energy rates for the renewable energy purchased over the contract term and earn the straightforward, compelling story of how their company runs on clean electricity. Energy market regulation and differences in markets across the country present drawbacks to this deal structure, though.

For a direct PPA to be possible, in general, the generating facility and the company’s operations must be located within the same grid region. Furthermore, only companies with operations in deregulated retail states can engage in this deal structure.

As only a handful of states have deregulated retail markets — and because most large companies have facilities across multiple grid regions — direct PPAs can constrain the extent to which corporations can procure renewable energy at scale.

Financial PPAs, like direct PPAs, are transacted directly between the generating facility and the corporate offtaker, but the crucial difference is that no renewable power is physically delivered. Consequently, instead of routing renewable power to the offtaker, the generation facility sells their renewable power directly to the grid and receives the open market price. The project developer pays the difference to the offtaker when the agreed-upon PPA price (or strike price) is below the market price, and vice versa. The financial component of this structure, is known as a contract for differences or a fixed-for-floating swap.

Corporate offtakers of both direct and financial PPAs can opt for a bundled PPA deal and retain environmental attributes (Renewable Energy Credits in North America) associated with the project’s energy production. With this option, corporations with sustainability targets in addition to financial savings goals can address both outcomes using a PPA.

Financial PPAs are often more flexible than direct deals and therefore appeal to many corporations because:

  • Buyers with multiple load centers across grid regions can satisfy renewable energy needs using fewer transactions.
  • Corporate buyers avoid affecting their utilities and transacting in the wholesale market only.
  • Technical risk and engineering problems are mostly mitigated since electricity is not delivered and developers take on most operational risks.

Although PPAs are an efficient way for many organizations to reduce their operational emissions, they are highly nuanced and require significant market awareness to return the greatest benefits. 

Considering a PPA for your company?  Contact our experts today

 

Previous Article
5 Takeaways from the BNEF Future of Energy EMEA Summit
5 Takeaways from the BNEF Future of Energy EMEA Summit

Last week, 18-19 September, at The Bloomberg New Energy Finance Future of Energy Summit in London, of which...

Next Article
Risk Strategies: The Real-Time Future
Risk Strategies: The Real-Time Future

Commodity markets in many deregulated states and countries have prices settle in increments as short as fiv...

NEW eGUIDE

A Practical Guide to Basic, Better, and Best Corporate ESG Reporting

DOWNLOAD