Skip to main content

Yokota Air Base Unlocks its Potential with State of the Art Microgrid

When Yokota Air Base entered into an Energy Performance Savings Contract with Schneider Electric, they made their mission of resiliency the priority. In a location prone to natural disasters, the base was in need of a more robust and consolidated control system, and an energy resilience plan. The solution? A state-of-the-art CHP Plant with microgrid controls, paving the way for a more independent, secure future.

Watch the video now to learn more about this groundbreaking project.