Decarbonizing Supply Chains Through Aggregated PPAs

aerial view of wind turbineAs world leaders met for COP27, it was already clear that alongside reducing emissions, the energy transition must consider how to mitigate power market volatility. While nuanced, Power Purchase Agreements (PPAs) are one avenue to provide long term stability to energy price fluctuations while enhancing sustainability performance. PPAs are an energy contract between an offtaker (a utility or corporate buyer) and a renewable generator for an agreed volume, price, and delivery structure.

Demand for PPAs is rapidly growing. In fact, the RE100 criteria now requires purchasing of renewable electricity generated from sites less than 15 years old. Consequentially, PPA demand and developer investment into new renewable projects are expected to increase. Simultaneously, as we will explore in this blog, new entrants into the PPA market are creating even more demand for these renewable projects.

Aggregated PPAs: a renewable solution for SMEs

Traditionally, PPA demand has been primarily driven by large corporations with significant electricity loads. Despite their willingness, renewable procurement is notoriously more challenging for Small-and-Medium Enterprise (SMEs) due to lower power demand, poor credit rating, and limited tendering expertise. This has left smaller organizations with limited options when it comes to renewable procurement.

However, aggregated PPAs can provide a solution that allows SMEs to gain economies of scale by working together on renewable procurement. In many cases of successful aggregated PPAs, a sponsoring corporation convenes a group of its suppliers into a buyer consortium to meet the volume demand required by a developer. This increases SME buying power, enabling them to access long-term renewables to reduce their Scope 2 emissions. At the same time, by enabling its suppliers to decarbonize through PPAs, the convening organization gets the benefit of reduced emissions throughout the supply chain, helping to address its own Scope 3 emissions.

Potential for PPAs to decarbonize supply chains

There are two possible PPA deal structures, both of which can be negotiated separately or under a joint venture:

  1. The convening buyer acts as the anchor tenant with smaller companies filling in to take remaining load from a renewable power project.
  2. Companies in a buying cohort enter an agreement on equal terms without a lead buyer.

Anchor Tenant aggregated PPA

With a growing emphasis on Scope 3 emissions, in the first structure, corporations are encouraged to use their size and influence to decarbonize their supply chain. By acting as an anchor tenant during PPA negotiations and offtaking a larger share of energy generated, corporations can help SME buyers who often do not meet the volume required by generators to finance a new renewable project.

An anchor tenant aggregated PPA often follows a 3-tiered approach, consisting of one large buyer, several medium-to-large buyers, and many smaller sized corporates. This helps large companies diversify their energy mix, thereby reducing risk, and small companies access the benefits of a long term PPA. The Energize pharmaceutical supply chain program, led by 15 global pharmaceutical leaders, has formed its first PPA cohort which intends to go to market with two sponsors as anchor tenants joined by seven participating suppliers.

Consortium aggregated PPA

A consortium of businesses can bundle their energy demand and enter an aggregated PPA together without an anchor tenant. Here, corporate offtakers unify to achieve similar goals: aggregate their energy offtake, benefit from economies of scale, and optimize their combined offtaker profile.

For example, as a part of its Project Gigaton, Walmart convened a group of its suppliers to execute a PPA with no anchor tenant. In another example, Philips, Heineken, Nouryon, and Signify came together to form the first pan-European aggregated virtual PPA without an anchor buyer. Schneider Electric was proud to advise these companies in their 10-year agreement that will avoid 230,000 tons of emissions annually.

Challenges of aggregation for offtakers

Alongside the benefits, an aggregated PPA will inevitably come with more stakeholders whose buy-in is required to successfully complete a deal. A PPA-buying cohort must confront conflicting motivations, priorities, and timelines that can slow down the decision-making process. Consortium offtakers should not only attempt to set shared and aligned goals with co-offtakers from the start, but also be prepared to compromise before going to market to increase the likelihood of a successful tendering negotiation.

Alternatively, a consortium can choose to nominate one buyer to manage the tender process and represent the best interests of all corporates. This responsibility often goes to the most mature corporation due to increased skillset for leading discussions.

The developer’s perspective on aggregated PPAs

For developers, a long-term power contract provides bankability, allowing them to secure debt financing. Additionally, diversified energy buyers help to democratize and increase demand for renewable projects, encouraging further investment.

Feedback from a developer focus group on the Zeigo platform highlighted challenges and some interesting insights:

  • Most developers do not have the legal resources to engage in different contracts for all corporates under an aggregated deal.
  • While a consortium is likely to produce favorable credit, a member with poor credit will influence a developer’s appetite for risk and willingness to engage in an aggregate PPA.
  • Developers may perceive less risk when consortiums consist of corporates from a range of industries, as market downturns will not affect the entire group to the same extent. However, this may complicate the desire for a uniform legal contract.

Outlook

The current energy crisis has increased operational costs of companies across nearly all sectors and geographies. Aggregated PPAs can help SME suppliers to secure renewable energy at a fixed price, mitigating price volatility and stabilizing operations to avoid disruption. These co-benefits of operational reliability and improved sustainability performance build a strong business case for all organizations to decarbonize.

While SMEs reap many of the benefits of an aggregate PPA, larger members too are incentivized by reducing emissions in their supply chain to meet their own Scope 3 goals. Plus, all parties benefit from price security, which is especially advantageous during a period of economic instability.

Although aggregated PPAs are still in their relative infancy and remain quite complex, they offer a tested and proven approach to system-wide decarbonization. As familiarity increases, challenges will reduce, and adoption will accelerate. Aggregated PPAs offer a helpful solution that benefits developers, large offtakers, and small offtakers alike, making them a trend that is ripe for growth.

Fill out the form below to get in touch with our team to better understand your opportunities.

Previous Video
Why Companies Are Joining the NEO Network
Why Companies Are Joining the NEO Network

NEO Network member, Scott Macmurdo, shares why companies are joining the NEO Network and how it can help yo...

Next Article
Are European PPAs Financially Viable in 2022?
Are European PPAs Financially Viable in 2022?

Price volatility and rising energy costs bring into question whether locking in a long-term PPA is a good m...